|
|
 |
Important Product
|
 |
 |

Honeywell Minerals Help Bottled Water Manufacturers Meet Demanding FDA Requirements
As consumers continue to seek healthier alternatives to soft drinks, there
is expected to be significant growth in the functional water, flavored water
and purified water markets over the next few years. Many of these waters
are re-mineralized with inorganic salts of potassium, sodium, calcium and
magnesium in order to provide functionality such as taste profile, and add-on
health and wellness benefits. A major challenge for producers of these
beverages is ensuring that they are in compliance with the U.S. Food and Drug
Administration’s (FDA) maximum bromate limit of 10 parts-per-billion in
drinking water. The existence of bromates in bottled water is often due
to the choice of ozonation as the disinfection method for the bottled
water. During ozonation, bromates can be formed when bromide impurities,
which are present in the minerals added to the water, are oxidized by
ozone.
Honeywell Specialty Materials has developed a range of low bromide minerals
to assist bottled water manufacturers in meeting the FDA’s standards. By
utilizing minerals that contain bromide in extremely low levels, bottled water
manufacturers can ensure that their products do not contain more than the
maximum allowable bromate levels. In addition to being low bromide,
Honeywell’s minerals are certified as kosher and meet the analytical
specifications of USP and the Food Chemicals Codex. Honeywell Specialty
Chemicals’ Riedel-de Haën brand products are manufactured at Honeywell’s
facility in Seelze, Germany, which is certified against ISO/TS 16949, ISO 9001
and 14001.
|
|
|
|