|
About Us - Honeywell Sterilant Gases
|
 |
Honeywell supplies non-flammable ethylene oxide sterilant blends for use by
healthcare providers and manufacturers. Sold as Oxyfume® blends these gases
have been proven to sterilize heat-sensitive medical devices with a higher
margin of sterility assurance than any other method.
When You Need the Greatest Margin of Sterility
Assurance
Oxyfume 2002 Sterilant is a blend of 10% ethylene oxide and 90%
hydrochlorofluorocarbon. It was developed to replace "12/88" sterilant
blends which were phased out in 1995. Oxyfume blends have been shown to provide
more sterility assurance than any other low temperature sterilant gas. The
following articles describe independent tests comparing several sterilant
technologies:
Alfa, M.J. and others, "Comparison of Ion Plasma, Vaporized Hydrogen
Peroxide, and 100% Ethylene Oxide to the 12/88 Ethylene Oxide Gas
Sterilizer," Infection Control and Hospital Epidemiology. 1996: vol.17:
pp.92-100.
This article presents data to show that 12/88 provides greater margins of
safety than do 100% ethylene oxide or hydrogen peroxide plasma units and it
also demonstrates the need to properly clean flexible endoscopes prior to
sterilization.
Alfa, Michelle J. and others, "Bacterial Killing Ability of 10% Ethylene
Oxide plus 90% Hydrochlorofluorocarbon Sterilizing Gas," Infection Control
and Hospital Epidemiology. 1997; vol. 18: p. 641-645.
This article presents data to show that Oxyfume 2002 performs as well as does
the 12/88 sterilant.
To obtain complete copies of each article, please contact Honeywell and request Sterility
Assurance Articles.
| Controlling Infection in the Healthcare
Center |
Sterilization is just one of many techniques for controlling infections in
a hospital environment. The following links highlight the growing concern for
infections acquired in healthcare centers - Healthcare-Associated
Infections[HAI].
Centers for Disease Control and Prevention [CDC]: |
|
|
| (The Rate of Nosocomial [Healthcare Center ] Infections Grows 36% in the
20Year Period Ending 1995.) |