We offer several Lumilux® after-glowing pigments that absorb daylight or
ultra-violet radiation to produce a variety of afterglow or
"glow-in-the-dark" effects for safety products as well as for toys and
novelties, suitable for use in paint formulations.
Our Lumilux® afterglow pigments are perfect to produce long afterglow
paints. We offer two different types of phosphorescent pigments for best use in
various matrix. There are zinc sulfide based products (N-grades), useable for
solvent based paints as well as for water based paints.
The rare earth-doped strontium aluminates (SN-grades) are only useable for
solvent based paints.
Most pigments can be used in accordance to the European Standard EN 71-3: Safety of toys - Part 3:
Migration of certain elements
The relative luminosity and long afterglow properties of pigments are closely
linked with their crystalline perfection, particle size distribution and the
transparency level of individual crystals. Incomplete crystal formation causes
cloudiness or mechanical damage to the crystals under high shearing forces and
fragmentation under pressure, which reduces the level of performance.
Phosphorescence of larger particles is more intense than phosphorescence of
smaller ones. However, Lumilux® long afterglow pigments are supplied in a range
of defined grain size distributions to meet the demands of various
applications. Finer grain size grades are not produced by grinding larger
particles but are synthesized independently under special crystallizing
conditions. As a result, this reduces the negative differential in luminance
compared with larger grain size grades.
Phosphorescent Water-Based Dispersion
Paints
To formulate an aqueous dispersion paint with a Lumilux® Green N pigment, use a
commercially available transparent paint. The best effect will be achieved by
mixing 120 parts by weight of the aqueous dispersion paint and 300 parts by dry
weight of the Lumilux® afterglowing pigment.
To prevent breakdown of the crystal structure in afterglow pigments, the mixing
speed should be very slow. If the paint is stored without being moved for some
time, settling might occur. This is a result of the high density of the
afterglow pigments but should not affect the quality of the paint.
Honeywell Specialty Materials can produce customized luminescent pigments to
customers specifications.
For further information,
please contact us.