|
Automatic Processes
|
 |
 |
Automatic Processes
The automatic sorting of letters and parcel post is an appropriate example
of automatic processes. The signal for the necessary alignment of the mail is
emitted by luminescent pigments added to the stamp ink or the printing inks
used in franking machines. The aligned letters and parcels can be printed with
the post al-code or their destination in the form of a luminescent line code.
This code gives a signal to a sensing device on the sorting machine.
Fluorescent as well as phosphorescent pigments are used for stamps and code
tapes. Phosphorescent materials have the advantage that excitation and sensing
can be carried out at separate points.
Lumilux® pigments are based on a variety of "host lattice" chemistries.
Zinc sulfide-based pigments, rare earth-doped strontium aluminates, rare earth
oxide sulfides, alkaline earth sulfides, silicates, tungstates, hexa-
aluminates, phosphates and a pool of organic heterocyclic compounds form the
basic chemistry of the Lumilux® product line.
Zinc sulfide-based pigments have been around for decades and bring many
advantages to the processes that utilize them. They demonstrate good fading
resistance under indoor conditions and their grain size distribution parameters
are adjusted to the most important processing methods. They show very good
fluorescent brightness performance, good initial afterglow brightness
performance and very uniform batch-to-batch consistency. For these reasons,
they hold an important place in the Lumilux® product family.
By using Lumilux® luminescent pigments with selected fluorescent and
phosphorescent properties, special excitation characteristic, optimized grain
size distribution and high signal strength, the wide range of Lumilux®
fluorescent and phosphorescent materials makes it possible to offer custom
tailored marking properties for most application problems.
Honeywell Specialty Materials can produce customized luminescent pigments to
customer's specification.
For further information,
please contact us.
|
|  |
|