Honeywell Refrigerants Europe

In Focus


Low global warming potential - SAE recommends Honeywell's coolant for vehicle air conditioning systems

This article was published in the February 2009 edition of AutomobilKONSTRUKTION

The research program of the International Association of Automotive Engineers (SAE) recommends Honeywell's coolant with low global warming potential for use in vehicle air conditioning systems in order to comply with the new more stringent regulations in Europe. According to SAE, coolant HFO-1234yf boasts excellent environmental properties and is associated with with the lowest risks. Detailed tests have shown that vehicles using this coolant consume less fuel and produce fewer emissions (greenhouse gases) than vehicles that use alternative coolants. The tests also showed that although one of the possible alternatives, CO2, had a global warning potential (GWP) of one. It was less efficient that the recommended coolant.

Honeywell
Phone: 05137 999-9411
E-Mail: sabine.chmielewski@honeywell.com