|
|  |
 |
Metal Panel Manufacturers
|
 |
 |
| |
 |
 Benefits for the Insulated Panel Manufacturer
Minimal Conversion Costs
Enovate blowing agent is a non-flammable liquid that can be rapidly deployed
in today’s manufacturing environments. Some minor modifications may be
necessary depending on how the current blowing agent is stored and routed
through the plant.
Excellent Processing
Feedback from users underlines the excellent foam system flow properties of
systems containing Enovate.
Environmental Solution
As a non-ozone depleting and non-VOC blowing agent Enovate is ideally suited
to replace HCFC-141b and HCFC-22.
Favorable Cost-In-Use
When examining next generation blowing agent options manufacturers have many
cost elements to consider when measuring the total cost implications of their
decisions. Some of the cost elements that may favor Enovate are :
Low conversion cost compared to
flammable and gaseous options
Possible foam density
reductions
Possible reduced panel waste due
to ease of processing
Handling Safety
Worker safety is enhanced through the use of a non-flammable blowing agent.
Risks to the facility and to the neighboring structures are
minimized.
| Enovate® Characteristics |
Liquid |
0 ozone-depletion potential |
Good solubility in polyols |
Non-VOC (USA) |
|  |
|
|
|