|
About Us
|
 |
In the mid-1980s, Honeywell (formerly Allied Signal Inc.) introduced
Spectra® fiber. An entirely new type of synthetic yarn, it was one of the first
commercially available extended chain, high-modulus polyethylene fibers.
Because Spectra® fiber is a polyethylene - with a carbon-to-carbon molecular
structure like that of a diamond - it creates a continuous filament yarn with
incredible performance and endurance. Pound-for-pound fifteen (15) times
stronger than steel yet light enough to float, Spectra® fiber is one of the
world's strongest and lightest manmade fibers. Spectra® fiber applications
include cut protection, ropes and cordage, vehicular and personal armor, and
fishing line, as well as various specialty applications.
The Spectra Shield® family of composite products began with the development of
Shield technology by Honeywell in the late 1980s. Shield technology was
originally developed utilizing only Spectra® fiber, but over the years
engineers have developed Shield products using other high-performance fibers
such as aramid fiber in our Gold Flex® and Gold Shield® products.
In the last 15 years Shield technology and the Spectra Shield® family of
composite products have revolutionized armor systems in ballistic resistant
vests and hard armor applications used by law enforcement agencies and
militaries throughout the world.
Honeywell manufactures Spectra® fiber and develops performance-enriched,
fiber-based technologies for applications where materials are mission-critical
and when success frequently means expanding the accepted limits of performance.
Honeywell does this serving as a technical resource to its customers and the
segments they serve.