Honeywell AZ-20 R-410A Refrigerant

Theory of Ozone Depletion

Theory of Ozone Depletion

What is Ozone?
Ozone is a type of molecule that is made of 3 connected oxygen atoms, which is written in scientific terms as O3. It is mostly found in the stratosphere, and absorbs harmful ultraviolet radiation that would otherwise find it's way down to us and cause a variety of problems for humans, animals, and plants. Stratospheric ozone is different from ground-level ozone, which contributes to smog in our cities.
 
How could CFCs and HCFCs Affect the Ozone Layer?
Ozone is constantly being made in our atmosphere, mostly by collisions of oxygen molecules (O2) and oxygen atoms (O). Ozone is also constantly being destroyed by similar collisions between O3 molecules and O atoms, resulting in pairs of O2 molecules. In theory then, there is a balance between creation and destruction that results in a constant layer of ozone.

The full names for CFCs and HCFCs are Chlorofluorocarbons and Hydrochlorofluorocarbons. CFC molecules are made of chlorine, fluorine, and carbon, and HCFC molecules also have hydrogen atoms attached. The widely accepted theory of ozone depletion is that these molecules, once emitted to the atmosphere, eventually are broken down over long periods of time into their individual atoms. The chlorine atoms then react with the ozone and cause ozone destruction to happen faster than ozone creation.

Why is Ozone Depletion Considered Bad?
Because stratospheric ozone protects us from harmful ultraviolet rays, ozone depletion means people, animals and plants are all affected by these rays when the ozone layer fails to stop them. This may include:

Increases in skin cancers
Increases in cataracts of the eyes which can result in loss of sight
Reduction in the yields of important food crops, according to some scientists
Why can't R-410A Affect the Ozone Layer?
R-410A is not a CFC or an HCFC. It is called an HFC, or hydrofluorocarbon, and is made of hydrogen, fluorine, and carbon atoms. Because it has no chlorine, it won't interact with the ozone layer once it breaks down.
Related Products

Genetron® Refrigerants

Honeywell Refrigerants Europe

Enovate® Closed-Cell Foam Insulation