|
|
Myths About R-410A
|
 |
 |
|
There have been a number of myths and misconceptions about R-410A
refrigerant and air conditioners that use it that we have heard over the years.
Some of these are completely untrue, and some are simply exaggerated.
Click on the one you've heard to learn more!
|
 |
1.
|
The higher pressures of R-410A are unsafe
Actually, air-conditioners that use R-410A are specially designed for the
higher pressures of R-410A. These systems have typically been rigorously tested
by their manufacturers, as well as by independent safety testing laboratories
such as Underwriters Laboratories.
Many dealers of air-conditioning equipment are not educated on the benefits of
this new refrigerant, and some use the "high pressure" argument to
convince consumers not to buy a product which the dealer isn't properly trained
to install or service anyway.
With over a million R-410A based air conditioners operating worldwide, and
nearly a decade of field testing and product history, there is no evidence to
suggest that R-22 systems are any safer than systems that contain R-410A.
|
 |
 |
 |
2.
|
The higher pressures of R-410A cause air conditioners to break down more
often
Evidence shows this is not only untrue, but that R-410A air conditioners can
be remarkably more reliable than air-conditioners that use R-22.
First, air-conditioners that use R-410A are designed to be heavier-duty, with a
thicker compressor shell. Usually this results in smaller, sturdier pieces of
equipment that vibrate less, putting less strain on the piping connections that
are the source of most leaks.
Second, most air-conditioner manufacturers require their technicians to be
fully trained on R-410A before they can sell or service that manufacturer's
R-410A equipment. As a result, the dealers and technicians that offer and
install R-410A are often better trained and have the right tools to give you a
more reliable installation.
One major air conditioner manufacturer who has been selling air conditioners
for over 50 years tells us that their R-410A air conditioners and heat pumps
are the most reliable systems they've ever introduced!
|
 |
 |
 |
3.
|
R-22 will be cheap and available through 2020
This is wishful thinking on the part of many service technicians. R-22 is
being phased out globally, and the manufacturing plants that make R-22 in
Europe, North America and other regions will eventually be shut down or
converted to make other chemicals. Just this past year, the 3rd largest R-22
manufacturer in the U.S. closed its facility.
In 2003 the U.S. EPA implemented an allocation program which limits both the
companies who can make and import R-22, and the amounts that they each can make
or import. This essentially"capped" the supply of R-22 in the
U.S.
In order to meet the reduction in use of ozone-depleting chemicals that
Congress laid out in the Clean Air Act of 1990, the U.S. EPA expects to pass
further laws before 2010 to reduce allocations of R-22 and other
ozone-depleting chemicals.
By 2015, the cap on R-22 and other ozone-depleting HCFC refrigerants will be
reduced to allow a maximum of about 60 million pounds of virgin (new) R-22 to
be produced in or imported into the U.S. Currently, the U.S. uses over 160
million pounds each year!
Forecasting the effects of these regulations isn't easy, but it sure doesn't
look good for R-22!
|
 |
 |
 |
4.
|
R-410A isn't the final refrigerant, and other new refrigerants are
coming
Every major air conditioner manufacturer in the United States has selected
R-410A as its choice to replace R-22 in new equipment, and there are at least a
dozen brands of R-410A air conditioners or heat pumps available today, with
more coming soon.
Why? In less than 3 years the U.S. Department of Energy will require a 20%
increase in the minimum efficiency of new home central air conditioners. This
means that air conditioner manufacturers will have to find ways to increase the
efficiency of their air conditioners. One easy way is to use a more efficient
refrigerant, and because the refrigerant 410A is at least 5% more efficient
than R-22, manufacturers can use R-410A to help them meet these energy
efficiency goals.
In other countries like Japan where the phase-out of R-22 is further along than
in the U.S. and Canada, the refrigerant R-410A is used extensively. The United
States is expected to follow their lead, allowing R-410A to become the global
standard. Honeywell is the world leader in developing and manufacturing
non-ozone depleting refrigerants, and we've never seen anything like R-410A,
and neither have our customers!
|
 |
 |
 |
5.
|
R-410A costs too much
It's true that non-ozone depleting refrigerants are more expensive to
manufacture. They use more expensive raw materials, are more difficult to make,
and aren't yet produced in the large quantities in which R-22 is produced. Over
the long-term though, manufacturing costs are likely to decline as R-410A
becomes more popular and is produced on a larger scale.
Also, in order to properly install and service air conditioners containing
R-410A, your air-conditioner equipment dealer had to invest in new tools and
new training, and part of this cost is passed along to you in your price for a
new R-410A system.
There are usually costs associated with new technology as well as with
protecting our environment. Air-conditioners that contain R-410A refrigerant
are likely to be slightly more expensive than air conditioners charged with
R-22 for at least the next few years.
Because of design differences between manufacturers, the cost to upgrade from
an R-22 system to R-410A can vary. There are at least 12 different brands of
R-410A air conditioners and heat pumps available in the U.S. and Canada
today, so you have many choices as a consumer. We recommend you research both
the equipment brand and the dealer you select to make sure that your choice is
appropriate for the quality of equipment and installation you want. Remember,
you do get what you pay for!!
|
 |
 |
 |
6.
|
R-410A technology is too new and risky
Air conditioners using R-410A have been available in the U.S. since 1995, so
they're not at all new. They're just new to people who haven't heard about
them!
Honeywell invented the refrigerant 410A over a decade ago, and it's taken
several years for some air conditioner dealers to learn about these products
and for some air conditioner manufacturers to design and offer their own R-410A
systems. Most manufacturers have had their R-410A air conditioners and heat
pumps on the market for several years.
Some contractors and AC dealers are rightfully concerned about selling
consumers on a refrigerant that might be discontinued. But this fear just
doesn't apply to R-410A systems anymore. Every major manufacturer in the U.S.
and Canada now offers a R-410A brand, and because of the terrific track record
of the reliability of R-410A air conditioners, it has quickly become the new
industry standard.
|
 |
 |
 |
7.
|
R-410A is new and may not be available to service your new air conditioner
if it breaks down
We've heard this line several times.
As the inventor of R-410A, Honeywell is committed to having ample supplies of
this refrigerant available, and started up a new $100 million manufacturing
plant to make sure that there is plenty of R-410A available.
There are at least 2 other refrigerant companies in the U.S. besides Honeywell
who offer their own brands of R-410A, providing both ample supply and
competitive pricing to air conditioning manufacturers and to service
technicians.
|
 |
 |
 |
8.
|
The lubricating oil used in R-410A systems absorbs water and makes systems
break down
Many air-conditioning contractors who haven't learned about R-410A often
hear this myth and repeat it to others.
Air conditioners and heat pumps that use R-22 use a mineral oil that circulates
through the system to keep the compressor and other parts lubricated. Systems
containing R-410A usually use a synthetic oil . Some of these synthetic oils do
absorb moisture more readily than mineral oils, but there are several reasons
why this is not an issue for home owners.
First, equipment manufacturers train their technicians to keep these oils from
getting exposed to the air where they could absorb moisture. As long as
technicians follow the manufacturers' directions in installing and servicing
R-410A systems, then the oil will remain clean and dry. These procedures may
also be required to make sure your warranty stays valid during the life of your
R-410A system.
Second, nearly all air conditioners and heat pumps that use R-410A have a
device called a "filter drier". This important part does exactly what
the name implies - it filters, cleans, and dries the refrigerant and oil as it
circulates through your system just like the oil filter in your car. This
device has been an important reason why air conditioners with 410A are
considered by some manufacturers to be the most reliable product they make.
|
 |
 |
 |
| |