|
What Makes R-410A a Better Refrigerant?
|
 |
What Makes R-410A a Better Refrigerant?
It's Environmentally Friendlier
If your system ever leaks, the escaping refrigerant won't contribute to ozone
depletion!
|
You Avoid the Risk that R-22 could Become Expensive or Difficult to Get
When your System Needs to be Repaired in a Few Years
|
| The old refrigerant R-22 will be phased out along with other ozone
depleting chemicals, and |
| both supply and demand of this chemical will be significantly affected by
current and upcoming regulations. By selecting an air conditioner or heat pump
that uses R-410A, you will avoid the risk associated with purchasing a product
that is destined to become obsolete. |
R-410A Systems Can be More Reliable than R-22 Systems
|
R-410A air conditioners and heat pumps are today's "state of the
art" systems, and utilize the most current technology available for
efficient and reliable operation. The heart of every air conditioner or heat
pump is the compressor, and newer systems are specifically designed to use
R-410A refrigerant. They often incorporate smaller, heavier-duty
"scroll-type" compressors that are quieter and operate with less
damaging vibration than older compressors that operate on R-22. Since R-410A
can absorb and release heat more efficiently than R-22 ever could, compressors
with R-410A run cooler than R-22 systems, reducing the risk of burnout due to
overheating.
|
It Uses a Synthetic Lubricant that Helps to Keep the System Operating
Smoothly
|
| All air-conditioning systems use an oil that circulates through the inside
of the system to keep all of the parts well lubricated, just like the engine of
your car. R-22 air conditioners use an oil known as "mineral oil" that
has been used for decades. R-410A air conditioners use newer synthetic
lubricants that are usually more soluble with the R-410A than the old mineral
oils are with the older R-22 refrigerants. This means the synthetic lubricants
and R-410A can mix and circulate more efficiently to keep the compressor and
other moving parts lubricated, reducing wear and extending their life. Also,
just as many new cars use synthetic oils because they are less likely to break
down under high stress and heat, the new synthetic oils used in R-410A air
conditioners are less likely to break down under extreme conditions. |
|
|  |
|