|
|
 |
On-Board Oxygen Generating System (OBOGS)
|
 |
 |
An On-Board Oxygen Generating System (OBOGS) offers significant advantages
over the traditional stored-oxygen systems used today on most high-performance,
high-altitude military aircraft and commercial airliners.
The on-board generation system is more reliable, safer and requires much less
maintenance than a comparable stored-gas system. In addition, stored-gas
systems have capacity limitations that simply do not exist with an
OBOGS.
In an OBOGS application, an adsorbent is used to remove nitrogen from the air,
which in turn enriches the oxygen concentration in the outlet air stream.
Materials such as zeolite are commonly used to remove nitrogen and concentrate
oxygen. Generally, these materials are produced as small crystallites, bound
with clay to form small beads. But the properties of the clay binder reduce the
effectiveness of the zeolite.
Honeywell has developed a new technique to bind crystallites using an organic
polymer as a binder, rather than clay, to achieve a higher zeolite
concentration. The use of this polymer provides an improvement in capacity,
since more sites are available for nitrogen to absorb.
The Honeywell approach offers an even more compelling improvement opportunity
by using an advanced ion exchange procedure to replace sodium ions with lithium
ions. Lithium-enhanced zeolite promises to provide significantly enhanced
performance and absorption capacity compared to zeolite with the customary
sodium ion.
|
|
|
|