|
|
 |
Traffic Alert and Collision Avoidance System (TCAS)
|
 |
 |
Since its initial flights in 1990 on board regularly scheduled, commercial
aircraft fleets, the Traffic Alert and Collision Avoidance System (TCAS) has
proven to be a significant factor in improved worldwide flying safety. The
system operates independently of, but compatible with, international air
traffic control systems and has been recognized by pilots and air traffic
controllers alike for its contribution to air safety.
The FAA has mandated TCAS for aircraft with 10 or more passenger seats
operating for hire in U. S. airspace. In Europe, ICAO has issued similar
guidelines for aircraft flying in the European Air Navigation Region and is
looking at a worldwide guideline for all aircraft with 19 seats or more by
January 2005.
Through cockpit displays and universally understood symbology, TCAS provides
flight crews with visual awareness of the location, relative altitude and
direction of travel of aircraft within a moving 40-mile radius. The system also
provides clear aural warnings and coordinated vertical flight commands in the
event of an airborne collision threat .
In 2002, Honeywell introduced the next-generation of collision avoidance
technology, the new Enhanced ACAS II (Airborne Collision Avoidance System) and
Mode S transponder system. ACAS II is essentially TCAS II with additional
software called "Change 7", which is the basis for the worldwide
requirement.
Building on these features, Honeywell has developed a number of advanced
technologies such as increased surveillance range options, superior bearing
accuracy, improved reliability and an advanced communication datalink, while
ensuring the system meets the full range of ACAS II and Mode S regulatory
requirements. A modular architecture assures easy upgrades to future
industry-defined systems such as ASAS (Airborne Separation Assurance System)
and ADS-B (Automatic Dependent Surveillance-Broadcast).
In addition to commercial applications, Honeywell has designed and developed an
Enhanced Traffic Alert and Collision Avoidance System (ETCAS) to provide
military aircraft operators with an extended surveillance range and the
capability to coordinate formation flying in addition to standard TCAS
operations.
Honeywell is the pioneer and worldwide leader in TCAS technology with over 40
years of Airborne Collision Avoidance System research and development
experience, including the first certified system in the industry. With
cost-effective, advanced technology and innovative designs, Honeywell has sold
over 10,000 systems to more than 130 airlines worldwide and 25 militaries.
|
|
|
|