|
|
 |
Enhanced Ground Proximity Warning System (EGPWS)
|
 |
 |
The two major causes of commercial-aviation fatalities - controlled flight
into terrain (CFIT) and approach-and-landing accidents (ALAs) - accounted for
80 percent of fatalities in commercial transport aircraft accidents in the
1980s. But over the last two decades, flight safety has improved thanks to the
introduction of Enhanced Ground Proximity Warning System (EGPWS)
technology.
CFIT occurs when an airworthy aircraft under the control of the flight crew is
flown unintentionally into terrain, obstacles or water, usually with no prior
awareness by the crew. This type of accident can occur during most phases of
flight, but CFIT is more common during the approach-and-landing phase.
The primary function of a terrain awareness and warning system such as
Honeywell's EGPWS is to reduce CFIT. The system achieves this objective by
accepting a variety of aircraft parameters as inputs, applying alerting
algorithms, and providing the flight crew with aural alert messages and visual
annunciations and displays in the event that the boundaries of any alerting
envelope are exceeded.
The system essentially monitors the airplane's location and altitude, providing
a map-type display of surrounding terrain and sounding an audible alert if the
airplane approaches too close to terrain, a body of water or a tall
structure.
The original GPWS concept relied on information from the air data system and
radio altimeter. Enhanced systems use data from satellite systems and databases
containing information on a digital elevation model (digital presentation of
the terrain elevation features on a topographic map) and an aeronautical
database.
As a result of EGPWS, the risk of controlled flight into terrain is now 50
times less in Western Europe and North America than it was in 1991, making this
one of the biggest success stories in the history of aviation. Since the
introduction of EGPWS in 1996, Honeywell has received reports of more than 30
incidents where the EGPWS gave an alert and provided pilots with timely
awareness of terrain in flight situations.
Honeywell has delivered more than 30,000 systems.
|
|
|
|